电路如上图,Voffset_CH1=0V,Switch_EN_CH1=1.8V(信号走直通),VOCM1=0V,信号源输入频率1KHz,幅度100mV的正弦波,在K2的3脚可以测到正弦波,但是LM5401的正负输出均为0(无输出?)。把VOCM1改为1.8V,正负输出都是1.8V。
对比了一下,原理图符号把LMH5401的6脚和5脚画反了,在板子上飞线改回来后,LMH5401还是没有输出。
请教一下,问题出在了哪里?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
yatao guo 说:对于LMH5401,单端输入,差分输出,如果信号从IN+输入,外部反馈电阻也接到FB+,会有正常输出吗?
这个没关系的,改变的仅是输出信号的极性
我用TINA仿真了下您的电路,可以正常输出,所以请从焊接或接线方面查找原因: