Other Parts Discussed in Thread: THS4561, LMH6626, LMH6624, OPA189, TLC2652
我用LMH6626和ths4561结合做了一个仪表放大电路,但是用万用表测试ths4561输出两端之间的直流偏置电压有3.7V,我想问一下是怎么回事呢,是ths4561这芯片坏了吗?这两种芯片我都是正负5V供电,恳请大佬解答一下,非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
上图中两输入信号需要与运放共地,不可以直接将信号源两端接在运放输入端
如果两输入都是0的话,VM2两端的电压是很小的。如果您这里的“没有输入”是指输入为0,VM2两端有电压3.7V,可能是芯片坏了
LMH6626很容易输出饱和的,可以测量LMH6626输出,看LMH6626是否输出饱和