Other Parts Discussed in Thread: INA128, LM331, LM231, OPA335
各位高手,我需要设计一个电路。有一个传感器,输出信号是一个正负1mV的直流电压信号。我需要将这个信号放大2500倍进AD。要求至少有14位的准确解析度。所以需要放大器具有非常好的稳定度。我曾用LTC1250零漂移运放。但是在2500倍的放大倍率下,稳定度也不好。并且分成两级放大,零漂会更大。请问各位高手有什么建议。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,对于微弱信号的输入,当用普通放大器增益设置容易导致高增益震荡的情况。建议使用仪表放大器,类似于INA128/9,外部使用电阻设置增益,最大10000倍。并且利用REF管脚设置输出电平。
你好!
由于是直流弱信号,故要尽量避免直接使用运放直接电压放大。建议使用精密运放(失调电压要小)先进行20~100倍左右的放大,然后使用VF转换芯片,推荐LM231,LM331,使用微控制器得出信号频率,进而计算得到相对应的直流电压值。其中,VF转换芯片具有低温漂的特性,使用数字的方法可以有效提高其抗干扰能力。
希望对你有所帮助。
正负1mV的信号,如果要求解析度为14位,则要求运放输入端引起的误差不超过0.12uV。(2mV/16384)
LTC的零漂为正负5uV。目前TI零漂最小的运放(OPA335)零漂的典型值为1uV。可以采用较准的方法消除零漂。
但一级放大器直接放大2500倍很容易振荡,可以采用在反馈电阻上加电容的方法进行补偿,可以消除振荡。
另一个方案,如果输出为差分信号,优选仪表放器,如二楼说的INA128是非常经典的仪表放大器,他的输入失调电压典型值为±10±100/G
其中G为增益,增益大时,等效失调电压会变小。