This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
AMC1200差分输入VINN是不是必须和电源GND1共地,还是说差分输入和供电电源可以是两路独立的电源。现在具体使用情况,VINP 2脚和VINN3脚是48V蓄电池经电阻分压后输入幅值在160mV,VDD1由另一路直流电源48V经DC/DC转12V,再经过5.1V稳压管稳压后给AMC1200供电,GND1为该直流电源的地。 在外部接线时48V蓄电池的正与直流电源48V正短接在了一起。上电后发现AMC1200频繁损坏,VINP1和GND1直接的电阻为2Ω。 想咨询这种使用是什么原因导致的损坏。
您好,您的这个电路有两个问题,
第一,输入是单端输入,VINN接地,B-和EGND还不共地是吗?那么VINP要提供+-250mV信号输入,或者建议VINN提供1/2VDD1=2.5V的参考。
第二,输出是单端输出, VOUTN接地,这个是不建议的,首先AMC1200设计的就是差分输出, 使用单端便会大大降低了信噪比。
可以参考AMC1311 针对单端输出, VOUTN接地的FAQ: