电路原理图如上,LMH7324的负输入电压由DAC7311来提供,现在这个板子调节VDAC电压(0.5,1V,1.25V),输入电压输入一个正弦波,1KHz或者1MHz都测试过,正弦波分别设置为对应VDAC电压的offset,1Vpp的幅度,但是比较器LMH7324的输出2脚和3脚都是高电平,没有任何电平变化。后面我把PNA5V改成了GND,两个输出还是高电平。
请问一下,是哪里有问题?VCCO不能接+5V吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
去掉LMH7324的输出串联电阻R112和R115,J11通过信号发生器33500B输入正弦波,正弦波的频率为1KHz, 幅度为500mVpp,Offset为1V。控制DAC7311输出VDAC=1.02V,用示波器测试输入信号以及LMH7324的输出3脚QA波形,如下:
通道2为比较器LMH7324的输出QA信号。
输出信号后的电路为:
把MUX36D04的A0和A1脚配置为00,MUX输出选择S1A和S1B。重新接上电阻R112和R115,再次测试LMH7324的输出,R112和R115两端电压都变为了5.09V,MUX36D04的输出DA和DB也都是5.09V。这里的电压PP5V为5.10V。
MUX36D04的输出TRIG_SIG_5V_P 和TRIG_SIG_5V_N通过一个电平转换芯片接FPGA的IO。
这里MUX36D04会影响LMH7324的输出,问题在哪里?怎么修改?