This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lmv331电流过大

Other Parts Discussed in Thread: LMV331

我使用LMV331做一个电压比较器,当电压低于一定电压时,比较器输出高电平,并保持。当单片机检测到后,由单片机I/O输出低电平解除锁定 , 但是有时候LMV331工作电流会为5到10MA,正常时候低于1MA。以下是原理图,麻烦帮忙看下一下是哪里导致的。。需要怎么改进,谢谢

  • 您好,测试10mA电流是VCC端的电流吗?有没有更换过芯片,重新试试? 我看到输出端OUT这里加了一个二极管和1K电阻到输入端,不知这里的反馈回路是什么意思?
  • 您好,10mA是VCC电流,芯片没有坏,如果重新上电,芯片是能够正常工作的。OUT脚加一个二极管和一个1K电阻到输入 端是为了让OUT输出高时电压能够反馈给放大器IN+, 使此时放大器IN+能够比IN-电压高,使OUT一直保持输出为高电平。直到OUT被单片机引脚拉低

  • 您好,您这里只提到OUT输出高时,反馈给VIN+,但是OUT和MCU接在一起,如果比较器输出为低时,接的MCU
    这里输出高,会产生短路电流到比较器的输出端。 另外,Vin+的输入滤波电容C3 这里也需要去掉,比较器的输入端加上滤波会起到反作用。