你好!咨询一款运放,输入电流0~1250nA,频率是50KHz。用TLC2201仿真时,如果输入2.5nA,波形还是可以的;如下图
如果输入1250nA,波形的上升沿和下降沿就差了许多。如下图,
不知是否有合适的芯片,推荐一下
又找了一下发现OPA132基本上差不多,只是VOS电压有点大,最大达到2mV,仿真也可以,再找找....
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,波形上升沿和下降沿看起来都比2.5nA的时候缓了许多,考虑到压摆率的影响。
给您推荐3fA输入偏置电流的精度运放LMP7721 ,SR能达到12.76V/us,并且这款也是Iib最小的精度运放,适用于对微弱电流放大的应用。
谢谢回复!LMP7721电源电压是+5V,在实际使用中,电流源是负压的,感觉还是±5V可靠些。又找了TI的芯片,好像OPA145和LMP7701也行,在Multisim14中不能找到这两个器件,因此不能仿真,不知是否能仿真一下?
您好,LMP7701在50Khz下确实输出失真,我仿真的波形中信号的频率没有达到50KHz,所以LMP7701在-3dB频率下的稳定带宽应该是不够满足您的应用的。其他几款高带宽的跨阻运放,我仿真了下OPA847 ,50KHz的信号频率是没问题的。
如果使用TINA 仿真85度环境下的波形,可在Analysis-Set Analysis Parameters 里去设置环境温度:另外,我这里也附上一篇跨阻运放的应用手册,看下如何计算-3dB闭环下的稳定带宽,从而您这边决定选择哪款作为您的应用:
不好意思,很久没上qq邮箱了……您发给我的qq号,我搜索不到……邮箱前面的数学也是我的qq,麻烦加一下……谢谢!