Other Parts Discussed in Thread: XTR111
你好.
目前正在使用XTR111在电路中,来输出电流信号.
输入端一切正常,输出端用万用表电流档测量,电流可以随输入电压变化而变化,但是电流却一直没有10倍放大,百思不得其解,请教大师,恳请给予支持.
电路用的就是DATASHEET的示例.且XTR111无错误输出,管脚8为高电平..不过MOS管的GATE管脚一直不是0V(不管电源电压如何变动).
注:不管电源电压如何调节(24V---5V), 输出电流都和输入电压信号一致,没有影响.
如:VIN=3V, Rset=2.5K,Iout=10*3/2.5=12MA, 但是实际输出是1.2MA, 然后VIN=3.5V,实际输出:1.4MA