This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE032底噪

Other Parts Discussed in Thread: AFE032

 AFE032的datasheet里提到的接收底噪是在放大倍数为32倍的情况下,请问是否有满幅放大也就是512倍情况下的底噪数据?

  • 您好,
    AFE032应该是不能工作在512倍的情况
    RX_PGA1 的输入电压范围是(AGND + 0.15) /gain ~ (AVDD – 0.15) /gain;
    RX_PGA2 的输入电压范围也是(AGND + 0.15) /gain ~ (AVDD – 0.15) /gain;
    那么假如RX_PGA1=32,RX_PGA2=16,
    这样,RX_PGA1 的输入电压范围是(AGND + 0.15) /32 ~ (AVDD – 0.15) /32,RX_PGA1 的输出范围就是AGND + 0.15 ~ AVDD – 0.15,
    而 RX_PGA2 的输入电压范围是(AGND + 0.15) /16 ~ (AVDD – 0.15) /16,因此RX_PGA1 的输出范围大于了RX_PGA2 的输入电压范围,AFE032就不能工作在线性区了
  • 感谢您的回复,那这样说的话不管AFE032的RX_PGA1调多大的倍数,RX_PGA1的输出电压范围总相近于它的供电电源范围是吧?也就是AGND + 0.15 ~ AVDD – 0.15,那这样的话RX_PGA2岂不是也不能调4倍和16倍,只能调到1倍?
  • 抱歉,是我假设错误误导了您,RX_PGA2是可以设置增益为4或16的,比如 AVDD=3.3V,AGND=0,如果RX_PGA1输出0.15V,RX_PGA2增益为16时,其输入范围是0.15/16=0.009375V 至(3.3-0.15)/16=0.196875V,0.15V在这个范围内,RX_PGA2可以输入0.15V,因此可以设置增益16

    那么请您检查下您的信号输入是否满足RX_PGA1和RX_PGA2的范围?

    另外,我在E2E论坛也看到了与您同样的问题,E2E论坛工程师回复的是将 RX_PGA 增益提高到设备的最大值没有意义,因为要考虑通过电源线将IR,耦合,传输线路损耗降至最低、通信距离等问题:
    e2e.ti.com/.../afe032-do-we-have-the-rx-noise-data-when-rx_pga1-32-and-rx_pga2-16