根据datasheet,TLV1704-Q1几乎可以完美替代LM2901A,
并且我注意到TLV1704-Q1比较器的“+”,“-”输入都有钳位二极管。这是否意味着只要满足这个输入的反向电流不超过10mA,比较器的输入就能小于-0.5V呢?
另外,这两款比较器还有其他的差异么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
根据datasheet,TLV1704-Q1几乎可以完美替代LM2901A,
并且我注意到TLV1704-Q1比较器的“+”,“-”输入都有钳位二极管。这是否意味着只要满足这个输入的反向电流不超过10mA,比较器的输入就能小于-0.5V呢?
另外,这两款比较器还有其他的差异么?
LM2901输入信号范围是 0 to VCC – 2,在VCC=5V时,其输入信号范围是0至3V,不可以输入负的电压,否则不可以正常工作;
LM2901的绝对最大额定输入范围是-0.3V~36V,输入-1V,超出了这个范围,超出数据手册中绝对最大额定值,就会永久性损坏产品
而TLV1704输入信号范围是V-至V+,即0~ 5V,在这个范围内都可以正常工作。
TLV1704的绝对最大额定输入范围是V- - (-0.5V)至V+ + 0.5V,即-0.5V ~5.5V都不会损坏产品
您好,目前就对在用的比较器LM2901做了此测试,输入信号(-0.3V, 0V),输出正常,输入信号<-0.3V,输出异常。
TLV1704是我今天才知道的一颗新料,我目前还只能通过datasheet了解,没有做过测试。
从datasheet来看,确实是有一个钳位二极管,我的理解是只要这个电流 < 10mA, 这个钳位二极管就会工作,从而保证比较器正常。如果如您所说,只要<-0.5V,比较器就会异常,那这里提及的diode-clamped是做什么用的呢
请问贵司有此类测试数据可以分享么