This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
我是用AMC1200做电流检测,VDD1 VDD2都由外部24V转换而来,其中VDD2由VDD1隔离而来。在断掉24V瞬间,AMC1200的输出会有一个12ms左右的脉冲,影响后端电路,请问有办法消除这个干扰吗?
以下是电路图:
黄色信号:电流
蓝色信号:输出电压波形
黄色波形:电流
蓝色:VDD1
粉色:VDD2
您好,
您测得的电流波形(黄色波形),是在AMC1200差分输出端测得的吗?您可以同时实测AMC1200输入端波形和其输出端波形吗?以检查确认这个脉冲干扰是从信号链的哪一部分引入的?从您测得最后一个示波器波形看应该不是从VDD1和VDD2电源引入的