This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA541: 驱动2欧负载,输出波形出现失真

Part Number: OPA541
Other Parts Discussed in Thread: OPA549

OPA541做大电流输出时,负载为2欧(运放输出端和地端之间),电路结构简单,同相放大,供电±15V,AC输入1KHZ,100mv峰峰值,G=4.调节增益,该失真并未消失。

  • 您好,

    您的增益电阻和反馈电阻是多少?您可以用示波器同时测量输入和输出信号吗?以对比OPA541对输入信号产生的作用

    根据您的描述,我用TI仿真电路是没问题的

  • 1k与3k,这个对比过,信号发生器出来的波形还是很OK的,是这样,我想了解一些你们有类似于这样的案例吗,关于OPA541波形失真的问题。我有点怀疑是芯片本身存在的问题(不确定),您们有关于一些大电流芯片的一些失真补偿措施之类的吗。仿真只是在验证理论,很多实际测量下,问题很容易发生,所以我不太明白这个OPA541驱动强载的时候为什么会出现这个问题? 

  • 您叙述说AC输入1KHZ,100mvpp,且G=4,但是您的波形输出是280mvpp或276mvpp,与您设置的增益对应不上?

    驱动的负载2Ω是纯阻性的吗?

    OPA541可以输出Peak current 到10A,我认为输出幅值280mV加在2欧姆的负载上,相对来说不是强载

    找到的一个与OPA541相似的帖子:

    https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/873273/opa549-negative-part-of-the-output-is-distorted?tisearch=e2e-sitesearch&keymatch=OPA541%2525252520The%2525252520output%2525252520waveform%2525252520is%2525252520distorted#

  • 你好,G=4,280mv是因为我在电路前面用电阻做了分压,实际上我把增益从2调制4,失真都在。2欧是纯阻性功率电阻。我发现幅值大小并没有影响到失真,所以有一些疑惑。

  • 你好,OPA541电路中,当G=4时,从手册上来看,带宽在400K左右,对应相位裕度有约70-80°。而且斜率已经是-20db/十倍频了,就算是不进行补偿,也不应出现这种情况,我看那个OPA549补偿电路,带宽被压的很低,输出加的15.9u电容作用不是很懂,麻烦解答一下。灵哇哦主要的问题:你认为针对OPA541这种情况应该怎么做呢

  • 您所附datasheet截图是OPA541开环增益相频曲线,判断稳定裕度需要看闭环下的增益相频曲线。

    还是建议您附上您所测异常输出波形的完整电路图

  • 下面文档给出了在电流限制期间提高稳定性 的方法,加上后看是否有所改善:

    IMPROVE OPA541 CURRENT-LIMIT STABILITY:www.ti.com.cn/.../sboa057