Other Parts Discussed in Thread: LMH6629
我想设计一个窄脉冲信号检测电路,脉冲峰值大约1mV,信号带宽大于50MHz。现在采用采用OPA855 设计一个同相放大电路,需要输入高阻抗,增益固定为30-40dB(信号放大40倍到100倍之间),-3dB带宽为100MHz。因为AC耦合的原因, 提供偏置电路,偏置阻抗Rin设为100K,反馈电阻Rf为120K(100+40/2)减小偏置电流导致的误差, 但是我放大一个10mV的信号 有点失真了。是不是Rf太大导致,我有几个疑问想请教下大家,1:是否需要AC耦合,因为不需要AC耦合偏置电路,Rf就不需要120K这么大!OPA855手册给的参考Rf最大为0.95K。2:如果需要AC耦合,怎么减小Rf,或者让信号时域不失真,AC仿真看着好像问题。3:传感器输出信号的脉冲宽度或者上升沿和放大电路的带宽有什么具体的关系,是不是输入信号上升沿不能小于3.3ns(三分之一的放大电路带宽(100MHz为10ns))。4:仿真的结果看电路是否稳定?相位裕度多少了?