This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我需要一个比较器电路,用运放的话速度上不去,所以使用了TL3016,我是用这个比较器做一个波形产生电路,相当于产生一个三角波,然后加到比较器上输出方波,方波反馈回波形发生电路从而产生三角波,使用运放可以完成,使用一些低端的能输出负电压的比较器也可以,但是使用TL3016就不行,我看手册发现这芯片只能输出正的和地。也就是不能输出负电压,有没有什么办法可以解决这个问题?或者说高速的比较器能够正负输出的还有哪些?
TL3016是经过整形的TTL电平输入,无法满足楼主要求。可以看下TL714 和 TLV3501。另外,楼主可以尝试slew rate比较高的运放。
请问楼主这个波形发生器的带宽指标?用途?
TLV3501和TL714都是单极性输出的比较器,不能输出负电,这个波形发生器想做到3M左右,目前用高摆率运放也只能使波形在1M的时候比较理想,1M以上就有轻微失真,再高就失真严重了
1、TLV3501和TL714可以正负供电,请仔细阅读手册。
2、使用积分电路做三角波形发生器是比较落后的做法,对运放的slew rate要求很高,需要选择高slew rate的运放。不知道楼主这个3Mhz的波形发生器的用途是什么?什么应用场合?如果是做signal generator,可以使用DAC+FPGA或者市面上的集成DDS信号发生器。