This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7321: LM7321MFX/NOPB技术咨询

Part Number: LM7321


你好!

      为了降低成本,目前采用TI运放LM7321MFX P2P替代ADI LT6205运放,但是输出无波形,在反相端测量波形与同相端相差较大。我们的输入信号是交流信号,频率大概2-3MHz,是不是有哪些参数需要调整?请帮忙指导一下,谢谢!

     以下是同相放大电路:

  • 您好,

    反相端和同相端的电压相差多大?一上电就异常吗?IN+端输入信号的幅值是多少,前端分压电阻是多少,图片比较模糊看不清

  • 前端分压电阻是指直流偏置电阻吗?分别是33R和8.2K。

    采用LM7321后,要有波形输出的话,这是需要调整IN-与OUT之间的滤波电容C1吗?

    1、以下这三个图片分别是LT6205的IN+,IN-和OUT的波形

    2、以下这三个图片分别是LM7321的IN+,IN-和OUT的波形

  • 单电源5V供电,输入信号范围就是0~5V,图中输入信号幅值都到6.88V了,看datasheet 7.1绝对最大额定值,输入/输出引脚电压为 V+ + 0.8 V也就是5.8V,输入6.88V运放肯定坏了

  • LM7321的电源电压范围V+,V-之间为35V。而且LT6205的输入电压范围V+,V-之间为12.5V都可以支持,同样采取单电源供电。

    没有那么容易损坏吧,会不会可能是在范围内出现波形失真?但也应该不至于波形畸变成三角波形。

    这款芯片支持单电源5V吗?规格书的表格有单电源2.7V,双电源±5V的描述,但没有5V单电源的参数表。

  • LM7321的供电电压范围2.5 V to 32 V,支持单电源5V供电,但是其输入信号范围与供电电源有关,最大输入信号幅值范围就是供电电源范围。

    绝对最大额定值也与供电电源有关,输入管脚电压最大值即为供电电压V+ +0.8V,超出其绝对最大额定值就会损坏。