我也想请教一下,如果这个电路是负电源,共模电压是如何看的?同时接地又是如何?即正极接地,负极为-48V。
226的供电是隔离电源供电的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
因为您要采集VBUS(-48V)电压,而VBUS电压的采集需要以INA226的地为参考点的,可测量的VBUS电压范围是0V 至 36V,因此是不可行的
我看您修改了VIN+和VIN-连线,其实这一点没关系的,VIN+和VIN-之间的差分电压可以是双极性的,也就是说正负都可以。
关于VBUS的连接,如我前面所述,它的测量是以INA226的GND也就是您连接的ISO_GND为参考点的。以您最新附的电路图为准,那么它测的是两个隔离地之间的电压,它们之间没有回路,我认为测出来的值没有意义。