This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO124: 手持信号仪给输入信号出现偏差现象

Part Number: ISO124

手持信号仪给输入信号10V,用万用表测试,只有9.8V,用电源给出10V电压,是标准的10V。求解

  • 您好,

    ISO124的输入电阻只有200kΩ,比较小,如果信号源内阻比较大,输入至ISO124的信号就会衰减明显。

    您使用的手持信号仪应该是存在一定的输出电阻

  • 手持信号仪的内阻为400KΩ,但是它的最大负载能有5mA,应该也可以啊,不解,求大佬指点

  • 手持信号仪如果给输入信号10V,实测只有9.8V的话, 其输出电阻不应该是400KΩ,您确认是400KΩ?

    信号仪存在输出电阻Rs,则实际输出的信号电压就会被内阻Rs分压一部分,输出的电压就是负载RL分得的电压,为Uo*RL/(Rs+RL)

    这样算,您的信号仪应该是有输出电阻约4kΩ

     

  • 还有个问题就是用手持信号仪输入,万用表测试其输入端电压时,可以观察输出电压会增大,应该是输入电压的增大原因,请问什么原因,求大佬指点迷津

  • 不太明白您的具体问题,你您的意思是用手持信号仪给ISO124输入信号,用万用表测试ISO124输入端电压时,其输出电压会增大?

    但是在您的源问题中是,手持信号仪给输入信号10V,用万用表测试,只有9.8V,输出电压是减小了呀?

    或者您可以再详细描述一下您的问题吗

  • 就是手持信号仪给输入信号10V,输出电压为9.856V,此是未加万用表;我添加万用表测试输入端的电压,输出电压增加到了9.87V,增加了20mV左右;求解

  • 仔细看了下ISO124工作原理,ISO124对输入信号的隔离,需要对输入信号进行调制才能通过这个1pF的Isolation Barrier,如下datasheet截图。输入放大器A1对输入电流和 ±100µA Ω 电流源之间的差值进行积分(An input amplifier integrates the difference between the input current and a switched 100µA current source. )

    我怀疑在用万用表测量电压时,万用表电池电压经过其内部测量电路应该会对ISO124的输入脚VIN一个输入电流,造成ISO124输出增大。建议您尝试用示波器测量ISO124的输入电压,因为示波器的探头输入阻抗很大,应该不会对ISO124造成影响

  • 示波器的探头也会产生影响,问题依然存在

  • 您使用其他信号源给ISO124输入信号,用万用表测试其输入端的电压,是否对ISO124的输出造成影响?如果使用万用表测试对其没有影响,那根本原因应该在手持信号仪上。我不确定您使用的手持信号仪到底有怎样的特性,对外接的负载或电路有什么要求,我想您需要咨询所使用手持信号仪的厂家的技术支持