This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在使用TL082C时发现,使用0-5V单电源供电,正相输入0-5V,反相接输出进行电压跟随,输出可以达到20mV-3.5V,这已经远远超出了规格书的性能,规格书中要求为双电源供电-5V,5V,输出到上下轨都有1.5V的差距。
又测试了TL082I,是不能像TL082C这样用的,必须双电源供电才能正常工作。
请问TL082C确实可以只用5V的单电源供电,并输出至接近下轨吗,还是我手里的这个批次的个别现象。
您好,
如下datasheet截图,TL082C和TL082I的最小供电范围是±5V,TL082C和TL082I的输入和输出范围是一样的,其输入和输出范围都有最小值和典型值,为了所有产品的一致性,建议设计电路时,都采用其最小值来设计,即其输入电压范围负电源轨4V以上,正电源轨4V以下;最大输出电压与负载有关。