Other Parts Discussed in Thread: LM837, TL064
如上图所示,MIC_2N和MIC_2P为具有直流偏置的差分信号,上图功能是实现MIC_2N和MIC_2P偏置电压的检测。按道理说输出电压Vo会跟随MIC_2N和MIC_2P的偏置电压,但实测输出不受输入的控制,很明显是运放自激了。如何对其进行相位补偿?保持运放工作的稳定性。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我试过了,没用。如果在同向输入端和反向输入端并接一个150ohm的电阻,则输出可以跟随输入,但会出现以下情况:输入端悬空时,输出电压应该是0V,而实际测得是1.6V,这是由什么原因导致的呢?我已经加了下拉电阻了,而且就算我把输入端直接短接地,输出是4V。
这是由于输入信号的直流偏置电压过低引起的。从datasheet中读出当LM837采用+/-15V供电时,Vom最小值为+/-12V,与电源轨相差3V,所以当采用单电源供电时,输入端信号的直流偏置要大于3V。希望可以帮到您!
另外,您所提供的电路图中所采用的TL064,对于这个料其实是一个道理,在采用单电源供电的使用过程中一定要注意提供合适的直流偏置。希望可以帮到您!