Part Number: THS4522
Other Parts Discussed in Thread: ADS1278
我的客户使用运放THS4522结合ADC ADS1278构成的模拟信号处理电路,输入范围0-5V,现在实际测试情况输入范围在0-0.4V时,采集结果一直是0.4V,其他频率输出正常,电路图如下,请帮忙查看是什么原因导致的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,THS4522的每个输出端容性负载能力为1pf, 您的问题应该是输出端接2.2nF电容这里的问题,差分端接2.2nF电容,相当于每个输出端对地接了2*2.2nF=4.4nF电容,虽然您这里的输出增加了端接电阻Ro, 隔离了环路增益的相移,恢复了相位裕度,但是同时也限制了带宽,datasheet中给出了负载电容Cl和端接电阻Ro的的推荐值,可以看到,当Ro=50ohm时,推荐Cload的值在50pF左右,按照您电路的接法,C12大概在25pF左右。您再验证下。或者您将C12去掉再测试下,引入Cload 会对电路产生震荡以及不稳定的情况。

您好,我用TINA仿真是没问题的.
您提到,其他频率正常,输出不正常时候,频率是多少?