This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3091功率合成问题

Other Parts Discussed in Thread: THS3091, OPA690

最近在做一个函数发生器,数字部分采用DDS输出所需波形后送OPA690射随器后,分成两路分别进两片THS3091(采用同相放大两倍后并联输出,输出采用小电阻连接至SMA头),问题是直接用同轴线连接至示波器时信号完全混叠,观察频谱无明显谐波分量,但是直接用示波器探头观察信号波形相当好,具体电路见附件

fre.TSC
  • 楼主你好!

    混叠这个词使用有误,混叠是采样的概念。建议楼主上传示波器波形。

    解决方法是:输入串45ohm电阻,示波器端用50ohm负载匹配。

  • 您好,早知道混叠会被尔等大牛指正,但实在找不到合适的词来表述了(波形很宽,就像眼图闭眼的那种状态),本人还是学生,对THS3091这种大电流,大电压高速器件的处理不甚清楚,换成两片OPA690后无明显问题,希望大牛们能提点小弟一番,不胜感激!

  • 阻抗匹配是为了防止反射。  THS3091-----50ohm------电缆-------示波器(示波器设置为50ohm输入阻抗),如果不能设置为50ohm输入阻抗,则使用无感电阻作为负载,有BNC接口的50欧姆负载,使用二通的BNC接头接在示波器端。