Other Parts Discussed in Thread: OPA561
用OPA561外挂MOS管做的压控恒流驱动器
OPA561是单电压+10V供电,输出外挂MOS,MOS参数是:50A 200V. MOS漏极串90V左右的灯串,最大电流3.5A。
供电DC100V左右。
当输出端用3米内的线接负载时时功能正常,用6米线接负载时输出纹波大,灯会闪。
期望做到输出线长6米时,接LED灯串,性能OK。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,输出端是否有串联小的隔离电阻,比如22ohm,100ohm以内的?
另外,6m cable除了有纹波,信号有没有衰减?
如果信号发生衰减,可能需要考虑加个buffer来增强驱动能力。