一个具有5V偏置的音频信号,音频交流分量大小大概1、2V。有个按键可以控制静音,那么如何做一个检测电路,检测静音呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
一个具有5V偏置的音频信号,音频交流分量大小大概1、2V。有个按键可以控制静音,那么如何做一个检测电路,检测静音呢?
henjun Chen,
您好,不是很明白您的应用。
1,您的音频信号送到哪里去呢?
2,当您的按键被按下之后,音频信号的输出就是0V了,那么您要检测这个按键是否被按下的目的是什么呢?
zhenjun chen 说:如上图,当按键按下时具有5V直流偏置的音频信号被拉到地,但我需要做一个电路来检测按键是否按下。那么具有5V直流偏置的音频信号应该通过一个什么电路来检测,达到检测出按键被按下呢?
如果仅仅是 “达到检测按键是否被按下” 的目的可以串联发光二极管。
在R167,S1的线路上串一个LED, 同时把R167改小即可。Q3的基集承受几个毫安的电流没有问题。
不影响偏置,检测音频的电路方法是:通过隔直电容取出交流信号,用运放检波,求出包络。再馈送到比较器。
Regards
Frank Pan