Other Parts Discussed in Thread: OPA2348, OPA2342, OPA2316, TLV2372
1:如圖in+ 增加,輸出增加2v就無法再改變(增加),是什麼原因
2:在datasheet 敘述可以知道是雙電源或單電源工作? ,及最小工作電壓
3:如此顆是否可推薦單電源,其他料號
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,当供电电压范围为3V~36V范围时,LM2904的每个输入端的电压范围为V-~(V+)-1.5V。也就是说当3.3V供电时,输入电压最大只能到1.8V。
输出幅值大小是和输出电流有关的,可以看下当Iout=5mA时,输出最大电压距离正电压轨典型值为1.5V,也就是说如果3.3V供电,Iout=5mA时,最大输出为3.3V-1.5V=1.8V。
所以如果您向抬升输出电压,建议提高供电电压范围,比如您如果想输出3.3V,那么供电电压至少3.3+1.61(Iout=5mA)=4.91V,也就是说至少5V供电或者更高电压供电。
2904是双通道的,双通道的rail to rail input和output的,8SOIC封装的,可以看下TLV2372,OPA2342,OPA2348,OPA2316等。