This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA365: 作为电压跟随器时,发现输出电压与输入电压产生了2mV左右的差异,请问是哪里有问题,如何解决呢?

Part Number: OPA365
Other Parts Discussed in Thread: INA333, ADS8331

  • 您好,

    运放做电压跟随器时,运放的输入失调电压会对输出产生一定的误差,但OPA365的输入失调电压最大0.2mV,您描述产生的2mV应该是其他原因产生的;

    在测量产生2mV误差时,OPA365的输入信号是什么,幅值和频率是多少?OPA365后级接的是什么电路?如果输出电流比较大的话,输出电压会有明显的电压降,具体见 datasheet Figure 7,如下截图:

  • OPA365的前级是一个全桥电路,前级的输入信号理论上是INA333的参考电压REF+(2.5V)加上两端的电压差与INA333增益的乘积,目前是在静态情况下测量的信号。

    OPA365的后级电路就是一个ADS8331的ADC,OPA365作为一个缓冲器接入到该电路。

  • 我现在测量的OPA365的前级电压约为2.512V,后级电压约为2.510V。

  • OPA365输入2.512V是在其输入信号范围内的,应该不是这里的问题;

    您断开OPA365后级电路,OPA365输出是否有改善?

  • 断开后级的ADC,还是有2mV的压差

  • 输入至OPA365的2.512V是稳定的吗?

    OPA365的供电电压是稳定的吗?

    您可以附上输入信号和供电电压的纹波测试示波器波形吗

    您测试了几块电路板都是这种情况?

x 出现错误。请重试或与管理员联系。