This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV3702: 同一块板子上,摘取焊接了四次不同的比较器,比较器型号都是tlv3702,相同测试条件但结果却不同,相差很大,求助

Part Number: TLV3702
Other Parts Discussed in Thread: LM393

这是一个倍压整流电路,测试的那条直线是二倍压输出,理论上二倍压输出应该为5v,结果只有一个比较器的测试结果接近理论值,剩下三个比较器都偏差很大,只在相同条件下同一块电路板上做了测试,在该板上摘取焊接了四个同型号比较器,四次测试结果偏差很大,且我自己排除了焊接问题,求问这是怎么一回事;个人猜测这几个比较器的功耗不同,只有功耗极低的比较器才能达到电路的理论输出,输出电压低的,功耗大,如果是我猜测的这个原因,那是不是我买的是假货;如果不是,请问有别的什么原因吗?

  • 您好,

    我需要先对您的问题做下确认:

    1、TLV3702是焊接在上面原理图中U1A和U1B 处了吗?即替代了LM393?

    2、二倍压输出应该为5v是指电路图中的V2吗?实际测量V2为多少?

    3、为了验证比较器是否正常工作,您可以分别给出所测试比较器各部分电压示波器波形吗?比如比较器两输入端、输出端、供电端波形

  • 1、原理图的LM393画的就是TLV3702,只是我没改名字,,,确实如您所问的焊接在原理图的U1A和U2B处

    2、二倍压输出应为5v确实是指电路图的V2,实际测量,替换四次比较器器件,结果都不相同,一个是4.96v,一个是2.82v,一个是3.9v,一个是4.4v,都是在同样的测试条件下, 在同一块板子上替换比较器

    3、测试过比较器各部分电压示波器波形,从波形上看,比较器工作正常,不正常的是整个电路的输出不正常,怀疑是每个比较器的功耗不同,导致电路输出偏差这么大,怀疑比较器买到假冒伪劣产品,不像正品那样功耗小;或者有别的什么我不知道的原因,想请教一下

  • 感谢您以上信息的反馈

    1、看您所附电路图,V4是TLV3702的供电电压,那么V4的输出是正常的吗?V4电压是多少?是否稳定,是否达到了TLV3702供电电压要求?您可以实测V4的电流吗,即实测TLV3702的供电电流是多少?以验证是否为每个比较器的功耗不同造成的异常;

    2、

    测试过比较器各部分电压示波器波形,从波形上看,比较器工作正常,不正常的是整个电路的输出不正常,

    这里说不正常的是整个电路的输出不正常,具体指哪里的输出不正常?仅V2电压吗?

    3、您是在TI官网TI store 购买的TLV3702吗,如果不是,那有可能是产品的问题;您可以在TLV3702的产品首页,如下截图申请TLV3702的样片吗,以验证是否您购买产品的问题?

    TLV3702的产品首页链接:

    https://www.ti.com.cn/product/cn/TLV3702?keyMatch=TLV3702&tisearch=search-everything&usecase=GPN#order-quality

  • 并不是在TI官网买的,仅V2电压不正常,V2电压输出低可能是因为整个电路负载大了,导致电压变低。个人猜测因为比较器假冒伪劣导致电路等效负载各不相同,v2电压输出情况也就各不相同

  • 我去试试测试v4的电压和电流情况

  • 好的,等待您反馈测试的结果