我想实现一个V/I转换电路,有推荐的吗?转成4-20MA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
看下下面链接中的示例是否有帮助,
Supply Voltage: 5 V dc
Input: 0 V - 2 V dc
Output: 0 mA - 100 mA dc