Other Parts Discussed in Thread: ISO124, ISO120, ISO121
ISO124应该可以传送直流信号吧?
为什么ISO120那么贵?
跟ISO124相差那么多?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ISO120和ISO121贵的原因是因为二者的Isolation Voltage Cont Peak (DC) (V)和Isolation Voltage Pulse/Test Peak 很高,在环境比较恶劣的工业上面应用更加安全。ISO121的Isolation Voltage Cont Peak (DC) 达4950V,Isolation Voltage Pulse/Test Peak 达到5600V。