This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LF347
LF347必须是双电源供电吗?
您好,
也可以单电源供电,LF347双电源供电范围是± 3.5V ~±18V,因此单电源供电的话,至少是7V;
另外,LF347不是轨至轨输入输出运放,因此使用的使用请注意输入输出范围。