This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA280-Q1: 数据手册上的一些问题

Part Number: INA280-Q1

question1:为什么INA280-Q1的零电流输出电压非常小,Max是GND + 25mV,而不是25mV ?

question2:数据手册上Output Voltage vs Output Current的曲线具体是啥意思,就是曲线的斜率是负载吗?并且手册上VS只给了三个测试值2.7v,5v,20v;那么当我Vs是10V时,输出电压是(Vs-1)V时,对应的输出电流也是在5-10ma之间吗?

  • 您好,

    1、应该是一种严谨的说法吧,GND上可能存在噪声;

    2、它主要表现的意思是输出电压降或者说输出电压摆幅范围与输出电流有很大关系,输出电流越大,输出电压范围越小,输出电压至电源轨越远;

    VS只给了三个测试值2.7v,5v,20v,是因为这三个值是INA280-Q1供电电压的 最小值、典型值和最大值。

    那么当我Vs是10V时,输出电压是(Vs-1)V时,对应的输出电流也是在5-10ma之间吗?

    看这个曲线,在高温125℃时,INA280-Q1是输出不了10mA的,它在大概输出7mA时,输出电压降就急剧增加;

    VS为10V时,您可以参考VS=5V或20V时的曲线,因为输出电流在5-10ma之间,VS=5V,20V时输出电压降曲线差不多一样