Other Parts Discussed in Thread: LMV339
你好,我的应用场景是:有一路标准变压1.65V,需要检测另外几路电压是否低于1.65V,有哪几种比较器可以选择?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我想只要1.65V满足比较器的输入电压范围,那么1.65V可以直接接比较器的一端作为参考,另一输入端给信号,如果Vin+> VIN-,则输出为高电平,如果Vin+< VIN-,则输出为低电平。 所以比较器的选择性还是很大的,下面是比较器的选型链接,您可以根据提供的电气参数进行筛选,比如供电电压最大最小值,需要几路的,传输延迟有么有要求等:
https://www.ti.com.cn/zh-cn/amplifier-circuit/comparators/products.html
LMV339MTX/NOPB比较器可以用吗?假设Vin+ 为被监控电压,VIN- = 1.65V,Vin+在某个时间点跌落到1.65V以下,持续n个us后又升到1.65V以上,比较器是输出高电平,低电平,高电平吗?
您好,我按照您的要求用TINA进行了下仿真,输入绿色波形是我随便建立了一个波形,3us之后幅值降为0,然后1us后又上升到1.65V。 仿真结果没问题。 注意LMV339是OC输出,所以输出需要上拉电阻到Vlogic。