Part Number: LM311
Other Parts Discussed in Thread: UC3825, TLV3501
输入正是100k的正弦波
输入负是100kHz的锯齿波
二者交截生成PWM波形
请问LM311能准确的交截生成对应的PWM波形吗
之前使用UC3525里面自带的比较器做的,LM311能达到这样的速度吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我用TINA仿真试了试,正输入时0~100Khz的正弦波,负输入时0~100Khz的三角波,然后输出上拉的是3.3V,仿真下来是没问题的。

谢谢,我在saber里使用LM311的模型是达不到这种效果的,我想问下lm311和uc3825里面的比较器的速度差别,主要就是在三角波交截生成pwm波上
您好,UC3825内部集成的比较器不知在UC3825的数据手册里是否有详细描述比较器的特性。可能需要您再去查阅UC3825的datasheet。
而LM311的最快响应速度达到165ns,可以说是一款高速比较器。
TINA基本上能真实反映器件的工作状态的,所以对于运放,或者比较器,如果能用TINA仿真是很方便的。
非常感谢,还有个问题请教一下,LM311和TLV3501的速度相比如何呢
LM311 和TLV3501 相比,TLV3501的速度更快啊,最快响应时间只有4.5ns呢。