This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1200: TI AMC1200的使用疑问

Part Number: AMC1200


我的电路图如下,使用AMC1200获取R11两端的电压差,我上电后,J13未接负载,我的R9电阻就冒烟了。

    是不是我这个使用方法不对?有推荐的电路?这个电路是用来采集汽车交流充电桩上的CP信号电压值?

  • 您好,

    J13的PE和+12V-1 、-12V-1电源是共地的吗?因为AMC1200的测量回路需要与被测回路共地;

    如果J13未接负载的话,TLP701的输出就经过R11,R9,然后AMC1200的VINP输入端,然后AMC1200PE的地,形成一个回路,相当于R11串联R9,再加AMC1200的VINP至地是TLP701 的OUTPUT 输出的负载,如果TLP701输出电流比较大或电压比较大的话,就可能烧毁这个回路中的元件。

    如果J13接负载的话,是否正常工作?请注意AMC1200的差分输入范围是±250mV; 共模电压最大为VDD1;VINP, VINN输入电压范围最大是VDD1 + 0.5V 。