Other Parts Discussed in Thread: TSB41BA3B-EP, THS770012, PGA281, LMH2832, LMH6401, THS7530
请问大神!项目设计中采用1394B通讯协议,信号速率100M-400M,输出的差分信号电压希望可调节,电压调节峰峰值范围0~1.8V,针对该要求可以使用哪款芯片?或者可以使用什么信号调理电路来实现该功能?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,您的意思是需要输出信号0~1.8V范围的是吗?可调节具体是什么意思,输出范围可调吗?
使用运放只能通过反馈回路实现输出和输入的关系,Vout=Vin*Gain。Gain可调。 您想通过什么可调,通过改变反馈回路阻值实现Gain可调,还是通过可编程增益器件实现可调?
您好,输出也要求是差分输出还是单端输出?如果也是差分输出,目前只有一款全差分可编程运放,型号是THS770012
单端输出的话,Gain=1.8/0.7,我看了下可编程运放的几个器件,它们的增益可调,但可能不能正好为18/7的倍数,比如PGA281,增益范围为1/8~128:
差分输出的可编程增益运放目前只有这一款THS770012,10dB的带宽为900Mhz。
可以用TINA进行仿真看看是否满足您的应用需求。
那可以考虑可变增益放大器VGA。比如LMH4.LMH2832,THS7530,LMH6401等。