This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL062: TL062 替换NJM062 输出异常

Part Number: TL062

客户有款机种,之前是用JRC的NJM062,目前是更改为TI的TL062;但现在产线发现一个问题,机子本来是用了10个用量,其中9个位置上没有变化,但有个位置却导致输出幅度大了5-8dB,更换回JRC 或者UTC 的062后,输出又正常了。帮忙分析下原因是什么 ?

  • 您好,可以对比下TL062和NJM或者JRC062的datasheet,看下二者电气参数的差异。

    TL062的输入失调电压在mV级,如果输入到TL062的信号幅值也在mV级的话,那有可能输入失调电压一起被放大作用到输出端,导致输出端幅值有提高。

    所以在选择运放的时候,尽量选择输入信号远远大于失调电压的运放。 可以看下JNM062的失调电压参数,二者对比下。

    或者将输入信号幅值增大,验证下TL062的输出是否正常。 

x 出现错误。请重试或与管理员联系。