This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1302: 输出有高频纹波

Part Number: AMC1302


图1 AMC1302电路图

图2 零输入时输出波形

采用图1所示电路测量电流,电流采样电阻为2.5mR(未标出)。在输入端无电流时,输出波形如图2所示。CH1和CH2分别为VOUTP和VOUTN,MATH1(橙色)为CH1-CH2。可以看到MATH1含有高频纹波,周期大概为1.6us,这个高频纹波导致后续采样结果波动非常大,

1)请问这个纹波是如何产生的?AMC1302的数据手册中并未有这样的波形。C1和C2两个电容都是1uF(没有加100nF),VDD1和VDD2都比较平稳,没有这样的纹波。

2)是否需要在后级加滤波器来消除这个纹波呢?加一阶低通滤波,其截止频率应该要小于100kHz了,带宽就达不到310kHz了吧?