Part Number: OPA454

你好,我用3.3V单片机输出PWM波形(也用信号发生器模拟输入波形),接线图如上图,OPA454采用单电源供电,OPA454没有放大波形输出,用示波器测量的信号比输入的信号还小,麻烦技术支持一下,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA454

你好,我用3.3V单片机输出PWM波形(也用信号发生器模拟输入波形),接线图如上图,OPA454采用单电源供电,OPA454没有放大波形输出,用示波器测量的信号比输入的信号还小,麻烦技术支持一下,谢谢
您好,看了下电路,首先SFlag引脚是OD架构,所以需要上拉电阻到VDD。
另外,输入共模电压范围最低为(V–) + 2.5。因此单电源供电,最低输入2.5V,如果您是0~3.3V输入是不符合最低输入电压要求的。
是的,如果0~3.3V 输入,双电源供电是可以的。
因为OPA454的输入不是轨至轨输入的,最低输入电压为(V-)+2.5V,所以单电源供电,V-=0V,至少输入2.5V。