This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH5401: LMH5401输出饱和信号负过冲问题

Part Number: LMH5401

TI 的技术专家 你们好:

        最近在使用LM5401过程中遇到输出饱和时负过冲严重问题。具体如下图示:

前级是TIA输出到T8、T9,如果TIA输出饱和后经LMH5401输出会有较大的负过冲;

黄色是5401输入,蓝色是5401输出,5401输出有较大的负过冲

用Tina仿真软件模拟,原理图如下:

如果信号源VG1、VG2输入幅值200mV,输出如下所示:

绿色波形输入,红色波形输出,输出产生负冲及振荡影响到输入了,

如果VG1、VG2输入改为50mV,则输出没有明显负冲过,波形如下:

当输入幅值过高时,LMH5401输出会负过冲??还是需要从电路哪些方面解决大信号输入时输出负过冲问题。

麻烦专家们抽空帮忙分析一下问题在哪里。谢谢!