Part Number: XTR111
我使用xtr111进行压流转换,输入是0~3.3V,输出理论上应该是0~10mA,但是我测量之后发现输出电流没有放大十倍,可能电流镜没搭好。然后电流也不是恒定的,我也不太确定我的管脚连的有没有错误,还是BJT选的不对。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,场效应管的D和S您这里是不是接反了?应该是D极接负载R13,您这里好像是S 极接的负载。 再确认下。
您好,是的,我看了下您使用的PMOS SI2309的数据手册,电路没有接反。
然后数据手册推荐的几款PMOS的型号Vgs电压在60V,SI2309的Vgs最大是20V,晶体管的电气差异比较大,而它是形成输出电流的主要部件。
所以我建议您更换和datasheet推荐的MOS电气参数相似的验证一下。