Part Number: OPA552
使用OPA552做同相比例放大,增益倍数为3,芯片供电为单电源30V时,空载电流约为6mA左右;双电源(+30V,-5V)时,正端空载电流为30mA,负端为50mA。改变负端电压至-4V、-3V、-2V时,正端负端电流会随之降低,-2V时正负端消耗电流在10mA以内,请问负端电流消耗大的原因是什么?双电源与单电源使用上有什么需要注意的地方?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.