This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High Speed Amplifier PCB Layout Tips

High Speed Amplifier PCB Layout Tips_sloa102.pdf
  • 简单翻译一下,器件的选型、地、旁路电容、信号通路。

    1,表贴元件,能减少寄生电感电容,而且能使布板紧凑;

    2,在电源输入端,使用钽电容,有利于滤除快关噪声;

    3,旁路电容,尽可能的靠近芯片引脚,有利于滤除高频干扰,降低谐波失真,而且多个旁路电容的“地”,尽量靠在一起;

    4,保持完整的“地”平面;

    5,去掉芯片引脚背面的覆铜,以降低寄生电容,对于反向输入引脚尤为重要,1pF的寄生电容,都有可能对运放产生很大的影响,甚至导致振荡;

    6,保持输入信号线尽量短、直,而且要做好阻抗匹配(50ohm或者75ohm);

    7,对于全差分运放,电路的走线,尽量保持对称;

    8,如果芯片有热焊盘,那么PCB要对应起来;

    9,在运放的输出端口上,串联一个小电阻,可以用于解决运放振荡问题,如果不用可以用0ohm直连。

  • 译得不错!