光敏二极管电流放大,参考官方推荐的OPA322设计(有修改相应的阻容参数),但无法达到1M频率。电流5~10uA ,频率 1MHZ,请问有没有其他的芯片可以满足要求?OPA322本身20MHZ带宽是无法实现该应用吧?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
光敏二极管电流放大,参考官方推荐的OPA322设计(有修改相应的阻容参数),但无法达到1M频率。电流5~10uA ,频率 1MHZ,请问有没有其他的芯片可以满足要求?OPA322本身20MHZ带宽是无法实现该应用吧?
您好,
您是参考下面链接中的光电二极管放大器电路设计的电路吗?您需要输出的电压范围是多少?也是单电源5V供电吗?您可以附上您使用的原理图吗
OPA322最大输出达不到电源轨3.3V,距离电源轨典型值10mV。如果您需要输出达到3.3V,您需要使用高于3.3V的供电电压。

您需要的最小输出电压是多少呢?光电二极管的结电容是多少呢?您可以根据上述链接参考设计中的步骤进行计算以确认运放GBW是否满足要求。