This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH5401: 放大倍数计算

Part Number: LMH5401

如图所示,LMH5401内部反馈电阻为25Ω,我了解的全差分放大器的放大倍数计算是,(175Ω+25Ω)/73.2Ω=2.73倍吗,为什么上图标示的放大倍数是12dB,也就是4倍左右呢?!到底是怎么计算的啊

  • 您好,

    这块需要考虑阻抗匹配的问题,因为信号源是输出阻抗为50Ω的信号源,负载是50Ω时其输出电压幅值才是Vs,这样信号源幅值是2倍的Vs,即2Vs。但是这里不是50Ω的负载而是137Ω,因此输出电压是2Vs*(137/(137+50)=1.465Vs,而不是50Ω时的2Vs*(50/(50+50))=Vs。 全差分放大器的放大倍数是(175Ω+25Ω)/73.2Ω=2.73倍,这样总的增益是1.465倍*2.73倍=4倍。