Other Parts Discussed in Thread: OPA569
如下图所示电路,我输入信号是50KHZ,幅值为320mV的正弦波,输出端的波形如图2所示,为什么电压没有放大,只有十几mV?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是的,但是-160mV已经超出了最低输入范围0.1V。
建议您用示波器实测放大器OPA567 IN+管脚信号实际是什么样的,看下是否为期望的输入信号,以验证所选耦合电容是否合适。
我筛选了下,供电范围一致的就是OPA569,但是输出范围和封装是和OPA567不一致的,如下截图
我在TI官网看了下,TI store有OPA567,您可以再下面链接申请样片:
https://tisamples.ti.com/order/tisamples/zh/search/?text=OPA567&searchType=
OPA567的供电范围是+2.7V to +5.5V ,如果接±5V,其两个电源端的电压差已经超过了其供电电压最大值,因此会损坏芯片。
从运放结构上讲,运放在工作时无法分清自己是被双电源供电,还是单电源供电。只要其两供电管脚满足其要求的电压差就可以正常工作。但是需要注意的是运放的输入和输出范围,其输入和输出范围一般都是与其两电源管脚电压相关的。