This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用opa2836搭了一个简单的电压跟随,我输入的1V的正弦波,从1hz到5Khz,按照数据手册来说不会有衰减,但是实际用锁相放大器测试下来,发现衰减非常大
请教大家
您好,
V5正极虚线标识的0V是什么意思?您搭建的电路中V5是输入信号是吗?那么这不是电压跟随器。运放同向输入端是VCC/4,V5是交流信号输入端Vin,那么输出应该是VCC/2-Vin,VCC=3.3V时,即Vout=1.65V-Vin。
用锁相放大器测试原输入信号(1V的正弦波,从1hz到5Khz)是怎样的?