Part Number: THS3001EVM
根据THS3001EVM搭建的电路,信号输入端口有波形,但是芯片反相输入引脚没有波形,反馈通路也没有波形,输出端测量有波形,且可以放大,这是为什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THS3001EVM
根据THS3001EVM搭建的电路,信号输入端口有波形,但是芯片反相输入引脚没有波形,反馈通路也没有波形,输出端测量有波形,且可以放大,这是为什么?
您应该根据运放虚短和虚断的原则去理解,虚短就是运放同向输入端和反向输入端的电压是相等的,就好像两个输入端短接在一起,但事实上并没有短接;虚断就是运放的输入电阻无限大,输入电流为0,就好像运放两个输入端之间断路,但事实上并没有断路。
在虚短和虚断的前提下,反向放大电路,输入信号在J2输入,电流流过R2和R4,流过运放反向输入端2脚的电流为0,这样电流流过R2和R4电流相等。同向输入端接地电压为0V,同时因为虚短,那么反向输入端电压也为0V。
根据以上,可以列出运放输出电压公式:
(VIN - V_)/R2=(V+ -Vo)/R4
代入V_=V+=0;且R2=R4;
Vo=-VIN
因此输出等于输入的反向,用示波器测量是有波形的;因为 V_=V+=0,用示波器测量的话,是没有波形的。