Other Parts Discussed in Thread: LMH6518, LM8272, OPA365
一个全差分运放LMH6518
给他的Vcm供给1.25V
而他的VCM Input Bias Current在ALL GAINS的情况下最大+-20nA.
请问可以直接用基准源供给么?
或者基准源+一个LM8272电压跟随供给可以么?会不会超过规定电流?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通常的全差分运放的Vcm 用来设定输出Vou+/-的DC水平,即平均高度。本身不会被运放放大,即如果输入1.25V,那么OUT就会被抬升1.25V。
所以这里的bias电流主要看会不会影响实际输入端的电压水平。 加跟随器可以实现低阻抗的输入,当然如果没有这么高要求应该可以不加,相对电源噪声或输出影响属于很低的水平。
当然LMH6518 如果有特别这样的要求请指正。