Other Parts Discussed in Thread: ADC3662
根据THS4521的手册第11页的,VOCM voltage range是1V~4V还是0.8V~4.2V?
另外如果ADC选择ADC3662,VCM默认就是0.95V,直接输出给THS4521即可? 如果0.95V不满足前一级运放的VOCM范围,就需要外接一个直流电平给ADC3662的VCM(比如1.0V)?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,您看的是VCC=5V的Vocm的范围。datasheet也给出3.3V supply的Vocm的范围:

同样可以看出,Vocm的范围和典型值的范围稍有差异,这是因为Vocm环路是一个独立的放大器,所以Vocm的范围供电电压之间的headroom是独立的。 3.3V或5V条件下,可以看出距离低压轨0V需要1V的headroom,即我们看到Vocm(min)=1V。 但是典型值这里又尝试去靠近低压轨0V,所以这里为0.8V。
所以我的建议是5V条件下,参考1V~4V。3.3V 条件下参考1~2.3V。
ADC的VCM=0.95V的话,我不建议直接接THS4521的Vocm。 可以看下其他运放是否有直接满足0.95V共模电压的。