This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3001: 搭建驱动电路带宽与芯片手册相差悬殊

Part Number: THS3001

采用ths3001搭建放大电路,负向输入1.2v,频率1MHZ的正弦信号,输出幅值仅为380mv。频率和波形不变,但与输入相比有较大延迟。但降低输入信号频率至100kHz,则输出幅值及相位与理论相符,无衰减和延迟,随着输入信号频率的增加,输出信号衰减会越来越大,相位延迟也越来越大。请问问题出在哪里?

  • 您好,我按照您的电路用TINA仿真了下,1M没问题,因为THS3001的带宽和压摆率都是足够的。并且可以参考下OUTPUT AMPLITUDE  VS  frequency的曲线,1M频率时输出幅度是没有衰减的。

    我看了下您的电路图,正负电压不知您是不是接错了,按照Figure61的引脚对应关系,上面应该是-15V,下面是15V,我看您正好接反,不知实际电路是不是也接反了呢?