你好,供电±50V时,E/D引脚通过上拉电阻方式使能输出,请问上拉电阻需要多大?和E/D_Com连接在GND和V-有关系吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
E/D Com是-50V,E/D 上拉100k电阻到+50V
E/D pin是以 E/D Com为参考点的,这这种情况下,相当于给E/D pin施加了100V电压(+50V-(-50V)),这超过了E/D pin使能电压范围( E/D Com + 0.8V ~ E/D Com + 5.5V),因此是不可以的。
如果您需要使用供电电压±50V来产生E/D pin的使能电压,您可以在供电电压之间使用电阻进行分压以产生E/D pin的使能电压。
如果还不明白,请回帖子。
1、若E/D Com管脚接-50V,E/D引脚如果以E/D Com为参考点来说,则其电压为3.19V,如果以±50V供电电压中间点0V为参考点来说,则其电压为(-50+3.19)V。
2、一共就这三种控制方法,其他2种被您排除了,只剩这一种,您为什么担心不够可靠?